norelem uses cookies to optimally design and continually improve the website. By continuing to use this website, you agree to the use of cookies. You can find more information about cookies in our Data protection declaration.okay

Clamping elements in the 04000 article group

go back

We clamp your workpiece

Clamping elements in the 04000 article group

Discover our clamping elements for workpieces and components to be machined in the mechanical manufacturing sector. Clamping elements from norelem are mainly used in the metal cutting industry, in general machine construction or on machine tools for mechanical production.

The selection of a suitable clamping element depends on the geometry of the workpiece to be machined, the required clamping force and the type of machining (clamping from top, side, inside or outside).
The type of actuation, e.g. pneumatic, manual or with a tool, also plays an important role.
Also the available space, the surface finish of the workpiece (is it a blank, machined,...) and the construction height for the workpiece to be clamped.
At norelem you will find numerous clamping elements adapted to your individual application.
Discover our range and order your clamping element comfortaby online.
Our technical customer advisors will also be happy to help you select the right clamping element.
Discover our multitude of clamping elements

Clamp straps

Example of use

04010 Clamp straps

To product

Clamp straps are used to secure objects unsuitable for the machine vice, to a work surface. They are designed primarily so that they can be easily adjusted to fit any workpiece.

Swing clamps

Example of use

04363 Mini swing clamps

To product

Swing clamps fixate workpieces on fixtures, plates and work tables. The advantage of a swing clamp is that they pivot away from the clamping area so that workpieces can be easily mounted or removed, guaranteeing an optimum workflow.

Side clamp

Example of use

04562 Side clamps

To product

Clamp and pull down a workpiece in one step with the adjustable side clamps and fixed jaws from norelem. The side clamp and fixed jaws form a functional workpiece vice with the added advantage of having a positive down effect to press the workpiece onto the rest.
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
CallbackDo you have any questions? We will call you back.display
Austria
Sitemap Print Recommended Newsletter Top
Copyright © 2025 norelem. All rights reserved. Tel. +49 71 45/206-44 to 45 · Fax +49 71 45/206-83