SolarCar

go back

SolarCar team from the Bochum University of the Applied Sciences

Students develop and build solar vehicle

SolarCar is a student project from the Bochum University of Applied Sciences, which is made up of students from different subject areas. Every two years, the team develops and builds a solar car, which is road-legal in Germany, in order to participate in different competitions all over the world. The highlight is the World Solar Challenge, which takes place every two years.
The SolarCar team from Bochum is one of the world leaders in the Cruiser Class and has already proved to be extremely successful: they came 2nd in the World Solar Challenge 2013, 1st in the World Solar Challenge 2014 and achieved remarkable success in the World Solar Challenge 2015. What's more, in 2012 the SolarCar team drove around the world in their solar car and earned a place in the Guinness Book of Records.
World Solar Challenge 2015
Every year, the World Solar Challenge, the world championship for solar vehicles, takes place in Australia. Teams from all over the world compete in a 3000 km race right across Australia. The SolarCar team competed in the World Solar Challenge in October 2015 with their sports coupé, the ThyssenKrupp SunRiser,and really impressed the jury:
3rd place in the overall ranking for the Cruiser Class
2nd place in the assessments for practicability and passenger kilometres
1st choice of the expert jury (the judge's commendation went to Bochum for the second time).
We would like to congratulate them on this success!
norelem in the project:
To build the ThyssenKrupp SunRiser, norelem sponsored the SolarCar team with indexing plungers for fixing the battery casing.

According to the rules, this battery box has to be quick and simple to remove for safety reasons.

To ensure this, the team opted for » stainless steel indexing plungers from norelem.

The casing with 60 kg of batteries and the accompanying electronics can be found in the rear of the SunRiser.