Model vehicle in the Karlsruhe Cooperative State University

go back
Model vehicle
in the Karlsruhe Cooperative State University
A shaft-hub keyless locking coupling from norelem was installed in a model vehicle as part of a student project by two students at the Karlsruhe Cooperative State University.
The Cooperative State University in Karlsruhe has the goal of integrating hybrid technology into model vehicles in order to develop one of the first hybrid model vehicles. Thus the two students in the mechanical engineering course of studies were working, among other things, on combining an internal combustion engine with an additional electric motor. The team consisting of Dominik Rauscher and Manus Ochs was advised by engineering professor Dr. Albrecht Nick.
A microcontroller making it possible to control both the motor and the engine was also programmed, and a new damping system adapted to the increased weight was developed.
Hybrid-Modellauto der Dualen Hochschule Karlsruhe
A self-centring shaft-hub keyless locking coupling from norelem was also used in the development of a second gearbox. norelem offers a keyless locking coupling that has a minimum space requirement and can be quickly fitted and removed with a central nut.

» 1 X 23370-050010 Shaft-hub keyless locking coupling

Hybrid-Modellauto als Studienarbeit der Dualen Hochschule Karlsruhe