Measuring facility for concentric running tests on a camshaft

go back
Measuring facility for concentric running tests

Bachelor thesis at the Technical University for Applied Sciences in Landshut, Bavaria

Measuring facility for concentric running tests on a camshaft

norelem supports the bachelor thesis entitled "Design, construction, final assembly and startup of a measuring facility for concentric running tests" by a student at the Technical University for Applied Sciences in Landshut, Bavaria.
During this thesis, a measuring facility was created for performing concentric running tests on a rim and a camshaft. This is used in the measuring technology internship of the Technical University for Applied Sciences in Landshut. Each year approx. 300 students complete the measuring technology internship and learn how to use state-of-the-art technology.
The use of standard parts is specified as a key focus area in design and construction. Using standard parts keeps costs low and reduces the time between design and completion of the project. Of course, as a supplier of over 30,000 standard elements, norelem supported the construction of the measuring facility.
norelem in the project: sprung centre sleeve
norelem in the project: fixed centre
norelem in the project:

The »sprung centre sleeve (33180-02) allows you to quickly replace the camshaft without having to use tools. This makes handling much easier, which is a welcome feature for the students.

The »fixed centre (33190-02096) is used on the counter bearing.