Supported projects

go back
Engineering Newcomer 2016
10/22/16 - Engineering Newcomer 2016
Next Generation Feeding System Blister wins the young talent promotion awardmore...
Device to optimise the posture
10/21/16 - Device to optimise the posture
Thesis at the HTL Waidhofenmore...
Camping trailer for an E-bike
10/15/16 - Camping trailer for an E-bike
Project work at the Stralsund collegemore...
System Engineering Project the NTB Buchs
10/15/16 - System Engineering Project the NTB Buchs
Two secret agents save the worldmore...
Construction of a lighting system
10/15/16 - Construction of a lighting system
Individual and flexible lighting systemmore...
Formula Student pre-event
7/11/16 - norelem Race Camp 2016 – Report
Hot wheels at norelem's first Formula Student pre-event.more...
nlm feeding system development project
6/15/16 - Automated feeding system
Engineering project at the Robert-Bosch-Schule in Zuffenhausen, Germanymore...
Measuring facility for concentric running tests
6/14/16 - Bachelor thesis at the Technical University for Applied Sciences in Landshut, Bavaria
Measuring facility for concentric running tests on a camshaftmore...
Grill instead of machines: norelem products with a difference:
Bon appetit!
5/20/16 - Rotisserie grill
Grill instead of machines: norelem products with a differencemore...
SolarCar
5/17/16 - SolarCar from the Bochum University of the Applied Sciences
Students develop and build solar vehiclemore...
Camera slider project
5/4/16 - Camera slider project
Construction of a camera slidermore...
Engineering Newcomer 2016
4/29/16 - Engineering Newcomer 2016
Engineering Newcomer is now in the third round.
Apply now!
more...
Gear wheel milling machine
12/15/15 - Gear wheel milling machine
Development of a gear wheel milling machine for milling gear wheels made from wood or plasticmore...
2015 Engineering Newcomer Challenge
11/12/15 - norelem and Cadenas selects the 2015 Engineering Newcomer
Cutlery wrapping machine machine impresses the panel of expertsmore...
Formula Student Munich: Look back at the 2014/15 season
11/6/15 - munich Motorsport
Formula Student Munich: Look back at the 2014/15 season.more...
10/9/15 - Construction robot system
Students are developing, designing and building a construction robot systemmore...
“Technische Fachhochschule Buchs” University of Applied Science
10/2/15 - “Technische Fachhochschule Buchs” University of Applied Science
Escape from Alcatrazmore...
Rear hoist
9/3/15 - Rear hoist
Students optimise a rear hoist for people with disabilitiesmore...
Akademische Fliegergruppe Karlsruhe aviation group project
8/27/15 - Akaflieg Karlsruhe aviation group project
Students research the flight mechanics of flying wingsmore...
The longboard project
8/12/15 - The longboard project
The challenge: to develop an innovative piece of equipment for an unconventional sporting pursuit, and get it ready for the marketmore...
F1 in Schools
6/29/15 - F1 in Schools
The "Keep on Running" team builds mini racing carmore...
Master's thesis: Milling fixture
6/24/15 - Master's thesis: Milling fixture
As part of his thesis Johannes Schneider designed a milling fixture featuring norelem components. By use of the milling fixture slots can be milled into a fabricated part.more...
Project Leonardo of the University of Applied Sciences Bielefeld
6/19/15 - Project Leonardo of the University of Applied Sciences Bielefeld
Students work up models adapted from sketches by Leonardo da Vincimore...
Estrobot
5/20/15 - Project: "Estrobot"
Optimizing a clamping systemmore...
ACTOR project
5/14/15 - ACTOR project from RWTH Aachen
Students test aerogels in spacemore...
Engineering Newcomer
4/18/15 - 2015 Engineering Newcomer
Engineering Newcomer is now in the second round!
Apply now!
more...
Solarthermische Entsalzungsanlage für Meerwasser
1/8/15 - STEAM 2000
Solar thermal desalination plant for seawatermore...
Formula Student Team munichMotorsport aus München
11/4/14 - Look back at the 2013/2014 season
Formula Student Munich: intoxicated with speed! more...
Hochschule für Technik Buchs Serve-Bot
9/24/14 - Serve-Bot: The small helper from the University of Technology at Buchs
A team from the Interstate University of Applied Sciences of Technology at Buch (NTB) were given the task of constructing a robot that, together with another robot could run a restaurant. norelem supported the project with a ball roller.more...
Team des Karat Racing Teams Formula Student
3/22/14 - Retrospective at the 2012/2013 season
The KaRaT team is the only one from the Rhineland-Palatinate and consists at present of over 40 students from various faculties of the Kaiserslautern University of Technology and University of Applied Sciences.more...
Design and construction of a 3-axis CNC milling machine for DHBW Heidenheim
3/11/14 - Baden-Wuerttemberg Cooperative State University Heidenheim: Milling machine
Design and construction of a 3-axis CNC milling machinemore...
Zahnstange-Ritzel-Versuchsstand
2/25/14 - Gear rack and pinion test station
The Institute for Control Engineering of the University of Stuttgart succeeded during the whole of 2013 in installing a test station. more...
Hybrid-Modellauto der Dualen Hochschule Karlsruhe
2/5/14 - Model vehicle in the Karlsruhe Cooperative State University
A shaft-hub keyless locking coupling from norelem was installed in a model vehicle as part of a student project by two students at the Karlsruhe Cooperative State University.more...
bubales puppet theatre
1/31/14 - bubales – Stage design for puppet theatres
Art teacher Shlomit Tulgan founded "bubales" – the first Jewish puppet theatre in Berlin – in 2011. "The driving force behind the project is to build bridges between cultures, strengthen the self-identity of Jewish children and to strengthen the laughing muscles of all the viewers", says Shlomit Tulgan.
norelem is supporting the construction of the new stage.
more...
Blasfolienextrusionsanlage der TU Ilmenau
1/16/14 - TU Ilmenau: BLOWMASTER Project Seminar
How Film is Made from Plastic Granulatemore...
Team des Formula Racing Teams munichMotorsport 2014
12/18/13 - municHMotorsport team celebrates successes
norelem congratulates the team on their first Overall victory.
The electric car pulled it off and drove to first place in the event in Spain at the Circuit de Catalunya!
more...
Solarthermisches Kraftwerk reech
12/11/13 - GreenAirEnergy
The Renewable Energy Challenge – "reech" for short – involved the task of building a power station by very simple means.more...
Roboter Akrobot
11/13/13 - Akrobot
"Akrobot" system engineering project of the Hochschule Buchs, Switzerlandmore...
Engineering Challenge
3/15/13 - Engineering Challenge »Originelle Maschine«
Du zählst zu den kreativen Köpfen von morgen?
Zeig's uns!
more...
Projekt Liegerad der HTW des Saarlandes
12/7/12 - Comfortable recumbent bike
norelem angle joints rides alongmore...
RACOON-Lab
9/17/12 - Grappling in outer space
How can a robot satellite in space recognise, control and grab objects?more...
Elektronikschule Tettnang Roboterschulungszelle
8/28/12 - Robot training modules
Up-and-coming technicians on automation course are supported by norelem products
more...
Hohentwiel-Gewerbeschule Singen Cubus Multifunktionsgürtel
6/4/12 - CUBUS multi-function belt
norelem supports technician projectmore...
Formula Student Team Darmstadt FaSTDa
5/10/12 - Start your engines
This year norelem is supporting the "FasDTDa" teammore...
Stallardo 11 der Hochschule Esslingen für Formula Student
5/24/11 - Stallardo '11
In 2011 norelem again supported young student engineers at the University of Applied Sciences in Esslingen in designing and constructing "Stallardo". more...